1/5/2018 5:06 PM | |
Joined: 9/27/2006 Last visit: 9/10/2024 Posts: 12282 Rating: (2683) |
Hello; The easiest communication functions to use between a S7-300 (your WinLC station) and a TIA Portal program is with PUT and GET functions. These are S7 communication blocks using server/client connections, that need only to be configured on one of the partners (the client). The following Application example shows how to set PUT and Get functions on the S7-300 partner, for exchnges with a S7-1200: https://support.industry.siemens.com/cs/ww/en/view/92269951 This link presents much information on S7 communication blocks with a WinAC MP station (also a SoftPLC from Siemens), including PUT and GET: Hope this helps, |
Last edited by: CS Moderator at: 1/7/2018 10:48:46 AMchanged link to attachment to a more permant one |
|
Follow us on