7/13/2022 2:04 PM | |
Joined: 12/18/2014 Last visit: 5/30/2023 Posts: 29957 Rating:
|
In attachment another suggestion. Instead the length not in cm but in mm. Counters works with double integers. So is the start value instead 10,000 cm then 100,000 mm. AttachmentConstant_calculation_of_the_remaining_length_8.3.zip (206 Downloads) |
This contribution was helpful to
1 thankful Users |
7/13/2022 2:13 PM | |
Joined: 12/18/2014 Last visit: 5/30/2023 Posts: 29957 Rating:
|
Yes, while the factor is 10 (mm instead cm) ... |
7/13/2022 2:25 PM | |
Joined: 12/18/2014 Last visit: 5/30/2023 Posts: 29957 Rating:
|
Here a version with a alarm output if the rest is lesser then 10,000 mm (10 m).
AttachmentConstant_calculation_of_the_remaining_length_8.3_V2.zip (230 Downloads) |
This contribution was helpful to
1 thankful Users |
7/13/2022 4:15 PM | |
Joined: 12/18/2014 Last visit: 5/30/2023 Posts: 29957 Rating:
|
A OR block? |
7/13/2022 4:18 PM | |
Joined: 4/28/2020 Last visit: 2/22/2023 Posts: 30 Rating:
|
Ok yes, sometimes even forgot the most simple things But the program will become kind of a spider web |
Follow us on