7/14/2022 2:37 PM | |
Joined: 4/28/2020 Last visit: 2/22/2023 Posts: 30 Rating:
|
No I just changed the value to give in, so I can give in in metres, multiply it by 100 for the calculations, but seems like the rest of the program isn't working well anymore AttachmentLeegloopdetectie_5.zip (234 Downloads) |
7/14/2022 2:46 PM | |
Joined: 12/18/2014 Last visit: 5/30/2023 Posts: 29957 Rating:
|
In the simulation it seems for me that it works correct. |
7/29/2022 1:58 PM | |
Joined: 4/28/2020 Last visit: 2/22/2023 Posts: 30 Rating:
|
Dear, I'm still working on the version with the counters, but I'm stuck again. For the moment, I change the start value manually on the TDE (here: 120000 mm). But I should want to change that value with two buttons (digital inputs). If i push one button, that value should increase with 10000 (10 m) and if I push the other it should increase with 100000 (100 m). Is there a possibility to do that? Thanks in advance AttachmentLeegloopdetectie_3_bis.zip (224 Downloads) |
7/29/2022 2:03 PM | |
Joined: 12/18/2014 Last visit: 5/30/2023 Posts: 29957 Rating:
|
No, there's no way for this. Because the start value can only changed by the display or remote. |
Follow us on