8/14/2012 4:17 PM | |
Joined: 8/31/2010 Last visit: 11/6/2024 Posts: 1523 Rating: (229) |
Hello Lars Andersen, Refer this comprehensive FAQ (including a webinar) on What are the prerequisites for migrating STEP 7 V5.x projects to STEP 7 (TIA Portal) V11?before proceeding. Another useful FAQ is What are the requirements for migrating a STEP 7 V5.x project to STEP 7 Professional V11? |
Like it? Rate it! |
|
8/16/2012 7:49 AM | |
Posts: 7 Rating: (0) |
I'm not sure, whether or notthe problem is my new PC with the TIA-portal V11 installed. I've tried to make a simple project with only OB1 containing 1 network with a simple SET instruction. But the TIA does the same. I've attached the .am11-file for this. Can anyone out there migrate it, to see if the problem is my TIA-installation? Thanks in advance Lars Andersen AttachmentMigration_test.zip (381 Downloads) |
8/16/2012 4:53 PM | |
Joined: 8/31/2010 Last visit: 11/6/2024 Posts: 1523 Rating: (229) |
Hello Lars Andersen, What is the exact version of TIA Portal v11 you are using currently? (You can find it by going to this menu Help -> Installed Software). You try installing TIA Portal v11 SP2 Upd4 and check for the same behaviour in case if you are using a different version. Currently I do not have the TIA Portal v11 installed in my machine, once I'm done installing shall update you the behaviour of the .am11 file |
Like it? Rate it! |
|
8/24/2012 7:14 AM | |
Posts: 7 Rating: (0) |
Thank you. I will now contact Siemens, to help me fix my TIA installation |
Follow us on