9/26/2019 2:13 AM | |
Posts: 3 Rating: (0) |
HELLO I FACE PROBLEM DURING CONNECTION TO RAMSEY MICRO TECH 9101 USING PROFIBUS PLC SIEMENS 313C-2DP / STEP7 5.5 CONNECTION FORM MICRO TECH TO PLC IS STARTED & NO FAULT ON CPU OR MICRO TECH PROBLEM CANNOT READ DATA FROM BLOCK 0 SUCH AS RATE ,LOAD ,SPEED ,TOTAL I TRIED TO SEND REQUEST THROW HEADER AS DESCRIBE ON MANUAL BUT NO SUCCESS. THANKS IN ADVANCE AttachmentRamsey-Micro-Tech-9101-9201-Reference-Manual.1.pdf (635 Downloads) |
10/13/2019 10:55 PM | |
Joined: 9/27/2006 Last visit: 1/15/2025 Posts: 12328 Rating: (2699) |
Hello Ahmed; Finding documentation on the implementation of the Profibus-DP protocol on the Thermo Fischer Micro-Tech 9100 is very difficult to locate. the closest I have found is this document: Thermo Fischer micro-Tech 300 Belt Feeder- Profibus documentation http://www.he-gmbh.info/media/pdf/1912975_pbus__3105.pdf The read and write groups that are required for data exchange by the 'Micro-Tech belt feeders are described in this manual, you should study them closely,. I might suggest also that you contact Thermo Fisher (Ramsey) and enquire if this document describes the required Profibus structure for the 9101, and if there is more up-to-date information on Profibus-DP for the 9100 serie. Thermo Electron, 501 90th Avenue N.W. Minneapolis, MN 55433 U.S.A. Tel (763) 783-2500 Fax (763) 783-2525 eng@thermoelectron.com In the recent past the forum has received questiojns on the Ramsey Micro-Tech 9101 Profibus structure, maybe the answers can help you out: Profibus communication Ramsey Micro-Tech 9101 problem?? Ramsey Micro-Tech 9101 read/write help?? https://support.industry.siemens.com/tf//ww/en/posts/ramsey-micro-tech-9101-read-write-help/187722?page=0&pageSize=10HHope this helps, Daniel Chartier |
Follow us on