4/18/2007 10:01 AM | |
Posts: 62 Rating: (2) |
My customer's having a problem about startup runtime. The problem started from the customer closed WinCC explorer, while the runtime is running. Thenafter he was trying to activate runtime again,WinCC try to activate for a while then goto deactivate automatically. I tried to resetWinCC byrunningfile ResetWinCC but the problem still the same. And also I had a look in folder diagnose. I foundWinCC tried to run but failed. However, I have not known the cauase of problem yet. Ihave attached the log file. Possibly anyone could help me to analyze theproblem. Thank you AttachmentDiagnose.zip (249 Downloads) |
4/18/2007 11:02 AM | |
Posts: 1084 Rating: (72)
|
Hi, Can you tell me how far it gets? Where does it stop activating? You could have a look at the following links: this this this this this and this not sure if your solution is there, but you could give it a try. with regards, Ikkezelf |
4/18/2007 12:32 PM | |
Posts: 3149 Rating: (171)
|
Hi which WinCC version are you using??? For WinCC 6.2 there is a hotfix for core2-processors.... http://support.automation.siemens.com/WW/view/en/24740694? Have already tried to start WinCC e.g. without activating scripts, Alarms,reports, taglogging.... during startup (WinCC > Computer > properties > startup)? nemo |