Industry Online Support
Technical Forum
8/22/2014 3:53 PM | |
Joined: 7/8/2009 Last visit: 9/20/2022 Posts: 56 Rating: (0) |
Dear Experts i'm facing same problem as this guy at this threadhttps://www.automation.siemens.com/tf/WW/en/Posts/94783 I have a system with 1) 417-5H PLC programmed using simatic S7 not PCS 7 2) WinCC V7.0 SP3 update 1 scada in server/client configuration. Network topology 1) 2 servers (redundant) 2) 3 clients. whenever i'm using 2 Servers and 2 Clients it is okay and the updating to/from the PLC is fine. But once i connect the third operator station the Delay time in updating the Tags to/from the PLC is around 25 sec. if disconnected this third Client station then the update time is okay and fine. I tried unistall then install again the WinCC but this didn't correct the situation.
|
This contribution was helpful to1 thankful Users |
8/26/2017 10:42 PM | |
Posts: 8 Rating: (0) |
Hello, did you find a solution for the problem? I have the same problem! |
Follow us on