7/29/2020 11:50 AM | |
Posts: 22 Rating:
|
I´ve got the same problem! but also with the huawei Mu609 Did you solve it? |
7/31/2020 1:01 PM | |
Joined: 12/12/2016 Last visit: 7/25/2025 Posts: 640 Rating:
|
Hello, We figured the Application example PDF is only working correctly with Image V2.2.0. If you want to use this method, you can send me a PM with an Email Address and I can provide you this Image. Configuration over iot2000setup requires some additional steps:
Kind Regards!
|
8/1/2020 5:50 PM | |
Posts: 9 Rating:
|
Hello Fe_lipe, I think I did correctly all what you mentioned (still with image V2.6.1), but without success! Please see the attached word file with the steps. I'm waiting for you to send me the image V2.2.0. Thanks! AttachmentIoT2040 modem configuration.docx (1053 Downloads) |
8/3/2020 1:28 PM | |
Posts: 24 Rating:
|
Hi Bergmanu, I have tried your last steps in the post, but I am still not able to connect. In fact, I have used the v2.2.0 but when I enter on iot2000setup / networking, I only see eth0 and eth1, no celular is defined. In the same line, when I type ifconfig, I only have lo, eth0 and eth1. Nevertheless, I have in my /etc/network/interfaces file the modem one configured. Please see attached the screenshots and the log file. It seems that the ttyUSB0 is lock by another pid… and that is why it is not able to connect. Best regards, Laura Attachmentmodem configuration IOT2040.zip (1048 Downloads) |
8/4/2020 8:05 AM | |
Posts: 22 Rating:
|
something is wrong... making all things that should work fine with mu609 but still unsuccefull results... |
Follow us on