7/14/2013 7:39 AM | |
Joined: 6/15/2012 Last visit: 5/15/2024 Posts: 18 Rating: (0) |
Dear All I have 2 pcs ofSIMATIC OP177B 6" PN/DP. In both the OPs all the 32 FUNCTION KEYS are not woking. If I press any of the FUNCTION KEYS, no action has been performed. This is happening in both the OPs. But TOUCH is working in both the OPs. IS IT A HARDWARE PROBLEM? or any configuration problem in software? Regards Rajib.
AttachmentOP 177B-datasheet-en.pdf (139 Downloads) |
7/14/2013 10:16 AM | |
Joined: 6/15/2012 Last visit: 5/15/2024 Posts: 18 Rating: (0) |
HiAyman Thank you so much. I will follow your instructions. Regards Rajib.
|
7/14/2013 12:57 PM | |
Joined: 6/15/2012 Last visit: 5/15/2024 Posts: 18 Rating: (0) |
Yes. Previously Function Keys are working to make screen changes. But now not working in both the OPs. |
7/14/2013 1:18 PM | |
Joined: 1/28/2009 Last visit: 9/10/2024 Posts: 6849 Rating: (1365) |
That is a bit strange.I suggest writing a support request for that and till receiving remedial instructions use an external keyboard if possible (D:\key_combination.zip ). Also check:
OP 277 FUNCTION KEY NOT WORKING |
Follow us on