6/19/2009 2:00 PM | |
Joined: 1/29/2006 Last visit: 11/1/2024 Posts: 447 Rating: (64) |
Hi again! I dont know, how reboot of MP277 affects the recipe handling. In my axperience, not at all. I would say, that something is "rotten" in your panel or in communication between panel and CPU. I would take following steps: 1. In CPU, I would insert a small program, which would simply controll critical recipe values. If they are outside of expected (=safe) limits, I would first limit them and then program a proper action (Warning, stop of machine, anything like that,....) and try to find out exactly, what causes this behaveour, if possible. I would also generate a message at every change of recipe value (in CPU!), so that you can later see, when does it happen.... 2. I would check the behaveour of your panel, all recipe settings, and also investigate this slow respond. I have seen, that you have had a discussion allready about this problem: /tf/WW/en/Posts/29689 Maybe you shold recompile your project and also download firmware on panel? I remember, that we have had the same problem (very slow responce)once, after conversion of older ProTool-Pro project in to WinCC flex project. It turned out, that problem was in acquisition cycle of some bigger array variables! have fun! uel123 |
Follow us on