12/10/2013 10:18 PM | |
Joined: 7/26/2012 Last visit: 5/17/2022 Posts: 15 Rating: (0) |
Hello, I'm quite a newbe here but I I,m struglling to connect a TP177A to my Stef 7, I'm using winccFlex 2008 with Step 7 V5.5SP1 My connection is a profibus between the panel and the CPU. In wincc I'm able to configure the panel but I can't transfer my project to the panel. The panel is started and configured with the right port. Any idea who can help me out? My configuration : 1. PS 307 5A 6ES7 307-1EA00-0AA0 2. CPU 315-2PN/DP 6ES7 317-1BH02-0AA0 4. SM321 DI 16xDC 24V 6ES7 321-1BH02-0AA0 5. SM321 DI 16xDC 24V 6ES7 321-1BH02-0AA0 6. SM322 DO 16xDC 24V/0.5A 6ES7 322-1BH01-0AA0 7. SM322 DO 16xDC 24V/0.5A 6ES7 322-1BH01-0AA0 8. TP177A 6AV6 642-0AA11-0AX1 DP/MPI/PPI RS422/485 Bootload 1.8 10-11-2006 Image V01.06.01.00_01.43 Flash Sizw 4MB Software AttachmentNetworksetup in winCC.pdf (112 Downloads) |
Last edited by: CyberJo at: 12/10/2013 10:26 PM |
|
12/10/2013 10:32 PM | |
Joined: 7/26/2012 Last visit: 5/17/2022 Posts: 15 Rating: (0) |
I forgot the screenshots from the connections in the Step7
AttachmentSoftwareversion.pdf (99 Downloads) |
12/11/2013 8:08 AM | |
Joined: 4/24/2006 Last visit: 11/6/2024 Posts: 8768 Rating: (1170)
|
Hello CyberJo, Perhaps this thread might help: /tf/WW/en/Posts/46604 And this one: how can you transfer a WinCC flexible project via MPI/PROFIBUS to a Windows-based panel? Best regards, Wizard |
Last edited by: Wizard at: 12/11/2013 8:47 AM |
|
This contribution was helpful to1 thankful Users |
12/11/2013 8:36 AM | |
Joined: 1/21/2013 Last visit: 10/23/2024 Posts: 4620 Rating: (708) |
Hi CyberJo, and if it can be of help to you: How can you transfer a WinCC flexible project serially to a panel? |
12/13/2013 11:49 AM | |
Joined: 7/26/2012 Last visit: 5/17/2022 Posts: 15 Rating: (0) |
HI, As far as I can recall, a straight connection : A1-A1 and B1-B1. I do not use A2/B2. |
12/13/2013 3:16 PM | |
Joined: 1/21/2013 Last visit: 10/23/2024 Posts: 4620 Rating: (708) |
Hi CyberJo, I think that channel 1 (Serial transfer) is disabled right? appears some error message in WinCC Flexible? is the "classic" control cables, etc. ..? you do not have, just to test the cable PPI/Multimaster? or this 6ES7972-0CB20-0XA0 Maybe you need to do this: How do you do an operating system update (OS update) on operator panels? |
Last edited by: Ste39 at: 12/13/2013 3:48 PMLast edited by: Ste39 at: 12/13/2013 3:35 PMLast edited by: Ste39 at: 12/13/2013 3:21 PM |
|
Follow us on