5/11/2007 4:38 PM | |
Posts: 1275 Rating:
|
Hi, There's a patch for v6.2 + dual core. If you're using this configuration install the patch and see is the problem persists. If it does: You said only WinCC freezes. is it a communication freeze, or does all of runtime freeze? What's your OS? Are there any other Siemens software on that computer, and under which versions? Is there anything in your logs, and can you post them here? Also.. check this out. Best regards, Danielle |
Last edited by: Danielle at: 11.05.2007 16:42Last edited by: Danielle at: 11.05.2007 16:40 |
|
5/11/2007 4:54 PM | |
Posts: 1084 Rating:
|
Hi, You are sure you don't have any network related issues? Often it's related to the setup of the network. with regards, Ikkezelf |
5/12/2007 2:02 PM | |
Posts: 36 Rating:
|
OK. On this project it is SINGLE CORE CPU WinCC V 6.0 SP4 (my mistake AttachmentDiagnose.zip (181 Downloads) |
5/14/2007 1:38 PM | |
Posts: 1275 Rating:
|
Hi, Here are a couple of things from your logs: // WinCC reported exception with code: C0000005 ACCESS_VIOLATION // Date: 25.4.2007 - Time: 16.27.6 // Caused at logical address 77124874 01:00003874 255,27.04.2007,08:42:07:343,1000005,4,josici,SZOJAUZEM,DataManager Runtime,Format error of tag 'Recipe_Silo4_MenjanjeBrzine'. Format ID: 0 = 0(hex) 255,27.04.2007,08:42:07:359,1000005,4,josici,SZOJAUZEM,DataManager Runtime,Format error of tag 'Recipe_Silo3_MenjanjeBrzine'. Format ID: 0 = 0(hex) 255,27.04.2007,08:42:07:375,1000005,4,josici,SZOJAUZEM,DataManager Runtime,Format error of tag 'Recipe_Silo1_MenjanjeBrzine'. Format ID: 0 = 0(hex) 255,25.04.2007,22:27:19:437,1007007,1,,SZOJAUZEM,SCRIPT,Alles vorbei INVALID_HANDLE_VALUE GetLastError() 1231 You should clear those out... Take a look at these posts: 1, 2 and 3, for the freezing problem. About access violation error. And about access violation and invalid_handle. Best regards, Danielle |
Last edited by: Danielle at: 14.05.2007 13:46 |
|
Follow us on