6/10/2011 6:49 PM | |
Posts: 241 Rating: (7) |
Please give us exact HMI/SCADA software you are using. Are you talking about WinCC? Check here Manual or Here for similar solution. |
6/11/2011 6:40 PM | |
Posts: 65 Rating: (0) |
I am usinng PCS7.1 SP1 With regards, Sumanta
|
6/11/2011 6:50 PM | |
Posts: 65 Rating: (0) |
DearSaravana kumar, I also saw these option but my question is when it takes backup .For example in windows you can configue taking backup every day say at 9PM or particular day in week etc . In case of WinCC archive when it takes backup to the particular configured folder ? How to schedule for backup ? With regards, Sumanta |
6/11/2011 8:12 PM | |
Joined: 2/6/2009 Last visit: 4/29/2024 Posts: 938 Rating: (118) |
Hi, Yes, We have the same option in the WinCC archive configuration to configure the start date and time also. This is already shown in my previous thread attachment. You can keep the maximum size of single segment as less value, so that the Time period covered by single segment will get more priority. Select one day for single segment and set the required start date and time in the Time of segment change settings for taking the backup every day. If you want to take the backup weekly once select theTime period covered by single segment as one week. |
_______________________________________________________________ |
|
6/12/2011 7:45 AM | |
Posts: 65 Rating: (0) |
Dear Saravana kumar Then what is the significance of time of the segment change option ? What could be the maximum size of each segment ? In my project I configured each segment 1 month and size of 3GB.Time period of all segment 1 year and size 36GB for (Taglogging slow /fast/message archive).What is your opinion regarding this setting ? When it takes backup in archive folder as I configured ? With regards, Sumanta |
Follow us on