12/30/2014 2:46 PM | |
Posts: 2 Rating:
|
Hi guys , Greetings to all and a Merry Christmas (and a Happy New Year) to the moderators of this forum, I am relatively new to the S7 plc programming but i had some basic troubleshooting and very basic programming while i was a technician over at a MNC running some moulding machines. I wish to rekindle my interest on S7. I wish to simulate the outputs using a simulator so that i can test my ladder programs without the need of a plc controller. I have managed to obtain a S7 software and i have installed it in my laptop running windows xp sp3. The software that i have installed is a S7 V5.4 SP3, no issues in the installation here. And i have also installed a S7PLC Sim Version 5.4. I hope anyone here can guide me on how to test a simple ladder prgrm and see the simulated results. How do i configure my laptop and how to set pg/pc interface and so on? I did try something on my own but when i try to add the plcsim v5.x into the list of modules installed i get an error stating " S7einstx.dll module can't be started. I humbly request that someone here can point me to the right direction or so? I got myself some help by someone sending me some notes on tia training document and i followed it step by step but the only problem arised when i started debugging in which i highlighted the OB1, clicked download but there was an error stating " a connection between your pc/pg device and the plc cannot be established" And i am stuck at that . Looking for some help so that i can learn a thing or two on some basic stuffs. Thank you and have a nice day. Rgds Ruben -------- New subject after splitting from Simatic Manager. |
Last edited by: Min_Moderator at: 12/31/2014 1:35 PMSplitted |
|
Follow us on