8/9/2010 9:48 PM | |
Posts: 14 Rating:
|
Hi, I use HSC to measure frequency from anemometer (frequencies are not to high, from 0 to about 120Hz). I guess I have configured everything just as I should, the address I have assigned is ID1012 and there is a simple question: is the value (in DInt datatype) in Hz, mHz (as in s7-200 or 300) or any other type? I need to know what value from ID1012 corresponds to 100Hz for example, to convert this value to meters/second. Thanks for answers, Artur. Splitted from HSC - high speed counters. |
Last edited by: maxdamage at: 8/11/2010 12:59 PMpart of this post moved to a new subject Last edited by: O_Moderator at: 8/10/2010 9:38 AMnew subject after splitting |
|
8/11/2010 12:07 PM | |
Joined: 9/23/2005 Last visit: 8/27/2024 Posts: 4347 Rating:
|
it is a pleasure to help you |
Denilson Pegaia |
|
Follow us on