12/26/2023 11:56 PM | |
Joined: 7/15/2009 Last visit: 1/2/2024 Posts: 30 Rating: (0) |
Dear Expert, please find attached detailed problem report about my problem , for CNC lathe machine the motor when have any signal to start moving ,, the motor only make vibrations. Attachmentproblem report.pdf (169 Downloads) |
Last edited by: The Helping Hand at: 12/28/2023 13:54:57Text formatting optimized |
|
12/29/2023 4:17 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872)
|
Hello abosama, Please note these are old drives & communication protocol with software is used to take up & restore parameters or is useful for horizontal communication. As such I suggest you to please refer the 611A drive manual's address link I shared in your earlier topic, chapter Main spindle module HS. Please study it, follow the steps, enter motor & drive related data correctly & carry out commissioning of drive & motor. You should be able to run motor with 611A drive independently & then it should be interfaced with main system. Hope this helps. |
1/2/2024 9:29 AM | |
Joined: 6/19/2017 Last visit: 5/27/2024 Posts: 8079 Rating: (165) |
Closed cause question posted twice. The second thread with the subject SIMODRIVE 611 configuration is published within the conference SIMODRIVE Converter system. Best regards, |
My Forum is the place to personalize your profile, |
|
Follow us on