7/12/2016 10:01 AM | |
Posts: 75 Rating: (19) |
Hi Antri, there is one documented requirement for Installation of SQL-Express: the Windows user Name of the user performing the Installation must not contain any space characters. Please double-check in WinCC V7.4: General information and Installation Hardware and Software requirements. (For Windows 10 there is only a restricted release of WinCC V7.4) Hope this will help you. |
7/12/2016 11:00 AM | |
Posts: 45 Rating: (1) |
I'm using Microsoft Windows 10 Pro (64-Bit) |
7/12/2016 11:42 AM | |
Joined: 5/12/2006 Last visit: 7/29/2024 Posts: 22326 Rating: (2999) |
and have you checked the windows event log or the install log file ? |
7/14/2016 1:27 PM | |
Posts: 45 Rating: (1) |
Do you have a link for the Windows 10 version? |
7/15/2016 9:10 AM | |
Posts: 648 Rating: (95) |
Dear Antri, additional you have software requirements from microsoft (Link to HP Microsoft) for SQL Server and you need a 64-Bit Version. With best regards rh1990 |
Last edited by: rh1990 at: 7/15/2016 9:11:04 AM |
|
7/21/2016 9:24 AM | |
Posts: 648 Rating: (95) |
|
Follow us on