10/8/2009 1:32 PM | |
Joined: 4/24/2006 Last visit: 8/23/2024 Posts: 8723 Rating:
|
Dear HassanShahat, Please have a look at this link: http://support.automation.siemens.com/WW/view/en/19109408 You can use a RS232/PPI multimaster cable or USB/PPI multimaster cable to transfer project. The mentioned USB PC adapter is not released to transfer project The connection between panel and CPU, can be using MPI cable. Best regards, Wizard |
10/9/2009 10:02 AM | |
Joined: 4/24/2006 Last visit: 8/23/2024 Posts: 8723 Rating:
|
Dear HassanShahat, Perhaps this link might help: http://support.automation.siemens.com/WW/view/en/23802404 Are you connected to HMI panel or is there a CPU in between? Best regards, Wizard |
10/9/2009 5:08 PM | |
Posts: 382 Rating:
|
Dear Hassan, Look at this link Hope this helps! with regards, how come? |
10/10/2009 12:09 PM | |
Joined: 7/3/2006 Last visit: 7/7/2024 Posts: 70 Rating:
|
Dear friends thanks alot for your help Now I get CP5512 Simatic net with PCMCIA to connect through my laptop I followed the instruction in the topichttp://support.automation.siemens.com/WW/view/en/23802404 exactly and when reading with the read in the "Diagnostics" I get the address set in the TP177A when putting in the transfer But till now can't transfer the project after setting every thing I tried the TP177A ( loaded with old application with CPU314 and communication port is working and data is transferred from and to unit with CPU ) Please still need your help Hassan |
8/26/2012 2:04 PM | |
Joined: 9/10/2009 Last visit: 5/23/2024 Posts: 4 Rating:
|
dear Mr. Hassan do you find solution for this communication problem or not?? regards Karam |
8/28/2012 1:09 PM | |
Posts: 3037 Rating:
|
Hello KARAM, Which configuration do you use? Do you use a TP177A too? Tweety |
Follow us on