7/2/2016 4:31 PM | |
Joined: 9/27/2006 Last visit: 5/1/2024 Posts: 12257 Rating: (2666) |
Hello e_skazem; Is this a new project you are developing, or a modification of an existing program? Are the drives communicating with the Profibus master at this time? For simple parametrization of the drives (quick commissioning) so they accept commands over Profibus, setting P700 and P1000 to a value of 6 is sufficient. See the following link, and the attached document; also look at the suggested documentation in the earlier posts in this thread. MICROMASTER 4 (MM4): Setting up an MM4 with a Profibus module https://support.industry.siemens.com/cs/ww/en/view/8894363 If this does not give you an adequate answer, maybe you should try to clarify the original question. Hope this helps, Daniel Chartier AttachmentMM440_420_settings.pdf (502 Downloads) |
Last edited by: dchartier at: 7/2/2016 4:32:06 PM |
|
7/4/2016 7:00 AM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hello skazem, If you have already read all the posts back like this below, and not like the PZD / PKW mechanism, try to inform you about DRIVE ES SIMATIC plus below from your Siemens dep. near you, their blocks are already made and it should be for you..... BUT is not free. MICROMASTER 4 (MM4), SINAMICS G120 (CU240S/D, DP/DP-F, PN ... Have a look table 3.4.1 Drive ES: DRIVE ES Engineering Software - Selection and ... - Siemens |
Last edited by: Ste39 at: 7/4/2016 7:01:28 AM |
|
7/4/2016 8:45 AM | |
Joined: 5/18/2015 Last visit: 4/27/2024 Posts: 98 Rating: (1) |
Thanks a lot It was useful document for me... |
SKAZEMCNC |
|
7/18/2016 9:57 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4774 Rating: (123) |
New question published by e_skazem is split to a separate thread with the subject 828D, CNC & PLC programing help. Best regards |
This contribution was helpful to1 thankful Users |
3/17/2017 2:18 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4774 Rating: (123) |
New question published by bolah is split to a separate thread with the subject Change MM420 to MM440, problem in output frequency. Best regards |
This contribution was helpful to1 thankful Users |
3/19/2017 8:36 AM | |
Posts: 2 Rating: (0) |
New question published by bolah is split to a separate thread with the subject Change MM420 to MM440, problem in output frequency. Best regards Thank you all the problem has been resolved, it was P2000 (reference frequency) that i later changed to 100.00 from 50.00 |
Follow us on