10/9/2023 5:50 AM | |
Joined: 4/28/2015 Last visit: 4/24/2025 Posts: 3345 Rating:
|
Hi, on the FS:07 IndOS is pre-installed on the eMMC and this is the first boot device. The IndOS needs to be configured and has no pre-configured IP address - see here for more information. To make it easy for you: Press and hold the USER Button directly with powering on the device --> the eMMc is skipped and it should boot from your SD card with Example Image. Then change the boot order in Example Image to boot from SD Card at first. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
Follow us on