8/3/2011 3:05 PM | |
Joined: 4/29/2010 Last visit: 3/19/2024 Posts: 1557 Rating: (161)
|
Hello, wich alarm number do you get at the panel? best regards |
8/24/2011 10:04 AM | |
Joined: 1/17/2007 Last visit: 10/6/2020 Posts: 289 Rating: (3) |
Hello, I already ordered the 24Mb card from Siemens and upgraded the PLC to the latest firmware v2.1.2. The connection works perfect between CPU1214C and TP700 via Ethernet. So.... 1. upgrade PLC firmware to V2 using 24MB SD card. 2. download latest TIA PORTAL V11 Update https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=de&objid=50085730&caller=view 3. you can start a new project with both the PLC (configured as V2) and HMI and compile/downoad to HMI only; download to PLC after firmware upgrade. |
8/24/2011 12:23 PM | |
Posts: 24 Rating: (1) |
Hi ionut.b, thanks for answering! I ve been working on it a little bit, and now connection works perfectly... but im getting this black screen... I was already working with V11 SP1 (is it the latest? ) Do you think that this black screen has something to do with the cpu running firmware 1.0? Unfortunately I dont have the 24mb sd card so I guess that I will have to go back to TIA V10.5 and keep in there :( Thanks! |
Follow us on