Industry Online Support
Technical Forum
11/15/2010 2:04 PM | |
Posts: 159 Rating: (3) |
Hello Cumulus!! I want to syncronize my redundant server pair with my clients. Do I really need to activate the "Syncronize over system bus" when all I want is to synconize over Terminal bus? I was hoping that all I neede to do was to activate the "Syncronize via Terminal bus (Slave)) on all clients... Splitted from Time synchronization of server and client wincc station. |
Last edited by: O_Moderator at: 11/16/2010 12:22 PMnew subject after splitting |
|
11/17/2010 1:42 AM | |
Posts: 2661 Rating: (279)
|
Hi Testermax, Have a look at the following manuals: SIMATIC Process Control System PCS 7 Compendium Part D - Operation and Maintenance Time synchronization (V7.1) Regards |
11/17/2010 12:26 PM | |
Posts: 159 Rating: (3) |
Hello Phantom75!! I have read through the documents you mentioned and I have the following settings on the WinCC red. servers (v6.0) and the clients (see submitted picture). There is a 10 min. delay in the time between the clients and the servers, but the servers are in sync. Should I use the "Use time from a specific computer" and point to the servers, on the clients instead? Man this really bugs me, it should suppose to be simple... :-) AttachmentTimeSync.zip (185 Downloads) |
12/27/2010 11:20 AM | |
Posts: 288 Rating: (22) |
No, Actually, I suggested to use the windows date&time sync feature available by default. |
Follow us on