5/22/2007 11:54 AM | |
Joined: 9/28/2005 Last visit: 12/14/2022 Posts: 414 Rating: (28) |
Hi, As mentioned by Helmut_13, your software is not the latest version. SP5 for Micro/win V4 can be downloaded from this site. As far as I know about most of the Siemens software the functionaly is not tested or ready for Vista. If you want to be sure I suggest you make a Support Request. Often it takes a few years before all industry software is suitable for a new OS. Please let us know what Siemens says about this. |
Smurf |
|
5/24/2007 9:53 AM | |
Posts: 10 Rating: (4) |
I have install MicroWin v4 SP3 on to my Vista laptop on Tuesday and it works no problems. They are a couple of warning stating to something is may not work, but I carried on with the installation. When I start up MicroWin it worked fine, I wrote a small program and download into my PLCdemo kit and it work ok. I even tried sucking(uploading) the program back to the laptop and it worked. I have not given it a good workout yet so I can not comment if it would crash after a while of being on, but if it starts up (on Vista) then thats a very good start. I have tried this Logo!SoftComfort on VISTA and it works see thread /tf/WW/en/Posts/9438 |
5/24/2007 10:35 PM | |
Posts: 13 Rating: (0) |
Thank you very much for your help. |
1/11/2008 11:08 AM | |
Joined: 9/28/2005 Last visit: 12/14/2022 Posts: 414 Rating: (28) |
Hi, With SP6 Micro/Win is Vista compatible. See http://support.automation.siemens.com/WW/view/en/27207727for download and information. |
Smurf |
|
7/26/2008 4:37 AM | |
Posts: 95 Rating: (10) |
If you are upgrading you may find this helpful too. I followed the directions and was able to upgrade from XP to Vista: There is also a link for LOGO Softcomfortupgrade to Vista) Pasted infofrom here: https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&siteid=cseus&aktprim=0&extranet=standard&viewreg=WW&objid=10805397&treeLang=en
You can begin with the STEP 7 Micro/Win software upgrade if the "microwin.exe" (or "microdos.exe") file is saved on your PC. |
Follow us on