Default Header
(header konnte nicht geladen werden)
2/26/2011 2:56 PM | |
Joined: 11/18/2009 Last visit: 3/22/2021 Posts: 14 Rating:
|
Hi, We have a 400-H project where we used Timestamp. We had some spare inputs in the SM321 which were not parametrised for Timestamping. During extension of the plant we re parametrised those inputs and connected extra signals. Every thing is working fine with the CPU 0 as Master. But when CPU 1 becomes Master (whether CPU 0 is STOP or RUN) we do not recieve the Timestamp info of the newly parametrised Inputs. How is it possible? In 400 H we need to have the same configuration/User program for both CPU, how this can happen and any idea where to check? Regards, Arunkumar Splitted from FB TIMESTMP (FB62). |
Last edited by: O_Moderator at: 2/28/2011 9:49 AMnew subject after splitting |
|
Follow us on