3/15/2011 8:01 PM | |
Joined: 8/31/2010 Last visit: 9/18/2024 Posts: 1521 Rating: (227) |
I installed in this order 1. WinCC v7.0+SP2 with no updates 2. WinCC v7.0+SP2 + Update 2 3. WinCC v7.0+SP2 + Update 2 When i installed update 2, i had the same problem. Surprisingly the problem was solved on the next day with no reason left for me to guess. Now when i am installing update 3 also i'm having the same issue. Today this error is no more in my PC, i don't know what's happening. Do you have more info on the SIMATIC Rights ? (will be helpful) You mean to say the current user shouldn't be in the Simatic HMI Group, am i rite? To add with I'm having a problem which is not allowing me to activate the Graphics Runtime alone. Refer this pdlrt.exe error. |
Like it? Rate it! |
|
3/16/2011 7:51 AM | |
Posts: 799 Rating: (43)
|
Hi, you will find all the infos about Simatic Rights and the needed user gruoups in this manual. I think this is everything you need to know! best regards |
Follow us on