6/6/2011 10:17 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
Hi RAM, Yes I too agree as it is quite large value. Can you explain me what is DIAMON? |
6/6/2011 10:22 AM | |
Joined: 3/3/2008 Last visit: 10/5/2023 Posts: 333 Rating: (51) |
hi find the attachment which explains about DIAMON with regards ram AttachmentDiamon.pdf (241 Downloads) |
6/6/2011 12:02 PM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
Hello RAM, I checked MD20100. Its value = X. Is it correct? |
6/6/2011 12:03 PM | |
Joined: 3/3/2008 Last visit: 10/5/2023 Posts: 333 Rating: (51) |
hi deep its correct. regards ram |
6/8/2011 6:32 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
HI Pee El Sea , So a single tool and a single cut will be correct….. YES Is there a turret index between the two steps ?...... NO. Is the index in the same direction ?......... NOT APPLICABLE. Can you change the program to cut one step and then the next without any index…….. NOT APPLICABLE. Can you change the order in which the steps are cut ?....... YES WE TRIED BUT ERROR IS SAME. Is the direction of the cut the same. ?..... YES. Are you always approaching from a positive X value to discount backlash……. YES Also I have worked on large lathes from 40ton cast rolls to oil shaft finishing lathes. Each has it's problems. What sort of lathe are you using and is this a new problem.?... YES IT IS BIG LATHE. SWING OVER CARRIAGE 1200mm, DISTANCE BETWEEN HEADSTOCK & TAIL STOCK 6000 mm, MAX WEIGHT TO BE LOADED 35 TON. Sorry lots of questions no answers .................. yet Pee REGARDS DEEP. |
Follow us on