11/24/2008 5:30 PM | |
Posts: 25 Rating: (0) |
And in this topic the issue seems solved : /tf/WW/en/Posts/18503 Siemens_Engineer_666 wrote: To resolve this issue, open your Registry Editor and add the following registry key: [HKEY_LOCAL_MACHINE\SOFTWARE\Microsoft\Updates\Windows XP\SP3\KB319740] Reboot your PC and you should now be able to install WinCC without any problems. Regards J Thank you so much, thar work fine under XP Prof. SP3. So, all i have to do is restarting PC bravelyI think ? But must i turn off automatic updates from Windows? (which probably contains SP3) |
11/24/2008 6:03 PM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
Hi See this instructions: regards |
11/24/2008 11:06 PM | |
Posts: 25 Rating: (0) |
Done SP3 removal, uninstall of WinCC and install again. But againattached problems.. Fresh installing XP SP2 and WinCC is solutioni think, formatting is a long way so i'm thinking of setting up XP with SP2 to D partition with only Simatic Manager 5.4 and WinCC 6.2 programs |
11/24/2008 11:07 PM | |
Posts: 25 Rating: (0) |
2 |
11/24/2008 11:08 PM | |
Posts: 25 Rating: (0) |
3 |
11/24/2008 11:09 PM | |
Posts: 25 Rating: (0) |
4 |
Follow us on