6/2/2011 2:46 PM | |
Joined: 5/28/2009 Last visit: 4/26/2024 Posts: 127 Rating: (10) |
Dear All... There are lots of threads which are not replay by any Experts in this Premimum Campaign. If any thread is wrong or reply allready, kindly mention it. I am giving some threads links bellow which is not answered by any Expet. Kindly answered thease thread links. Is it possible to use a ramp with multiplexer ? crc error in modbus communication FM351 Diagnostic MultiComputing Problem inmadiatly CPU makes a Full Shutdown of the F-Program during startup we want to do data logging from the PLC through two ports cp2433 which is still in "RUN" Quarterpounder or Royale with cheese in WinCC flexible |
Last edited by: MavEric at: 6/2/2011 3:47 PMRegards, |
|
This contribution was helpful to5 thankful Users |
6/2/2011 2:56 PM | |
Posts: 691 Rating: (36) |
Well its not about the Premium Campaign. If you look at the Thread Starting dates then only one thread come into picture we want to do data logging from the PLC through two ports Also I must admit that the threads are mind confusing |
6/2/2011 3:08 PM | |
Joined: 5/28/2009 Last visit: 4/26/2024 Posts: 127 Rating: (10) |
Hello... We need reply only on the above threads weather the threads given before campaign or after. |
Regards, |
|
6/2/2011 3:24 PM | |
Posts: 38 Rating: (0) |
Yes I agree with MavEric in this issue.If any normal member cannot give answer to the above theards then Expert should take care of thease kind of threads. |
6/2/2011 3:27 PM | |
Joined: 2/6/2009 Last visit: 4/29/2024 Posts: 938 Rating: (118) |
Hi, Good intiative. Thank you for it. Let me have the look into the thread.
|
_______________________________________________________________ |
|
6/2/2011 4:23 PM | |
Joined: 8/25/2006 Last visit: 5/3/2024 Posts: 2203 Rating: (277) |
Hello. Let me give you a link to the feedback from moderators: NO REPLY not satisfied. I think this feedback also valid for the experts. |
Last edited by: KSN at: 6/2/2011 4:24 PM |
|
This contribution was helpful to4 thankful Users |
6/3/2011 7:40 AM | |
Joined: 5/28/2009 Last visit: 4/26/2024 Posts: 127 Rating: (10) |
Thanks....KSN I would like to bring the following points into your consideration. Firstly as I have mentioned that there are many threads which are left unansawered in this premium campaign against which you have given a link to a thread for my reference.On going through that link I found out that the mentioned thread does not fall under the preimium campaign catogry so my question is still left unanswerd and the moderator also mentioned there that the forum members might not have time o reply each and every thread. Secondly please see this link Ranking List This thread falls under the Premium Campaign catogry and will find that this thread is for Umencho expressing one's respect for him which got almost 41 replies which is good and i myself agree that Umencho is a great person and an expert but the amount of replies for this thread clearly shows that the forum members do have time to reply but still some threads are left unansawered. |
Regards, |
|
This contribution was helpful to1 thankful Users |
Follow us on